Package empro :: Module empro :: Module core
[frames] | no frames]

Module core

all core and basic functionality.

Classes
  ApplicationInfo
Interface to meta information about the application such as the exact version, possible expiration dates, ...
  ApplicationPreferences
No documentation available.
  Attributable
Interface to a attributable objects.
  BooleanExpression
No documentation available.
  Camera
A virtual camera object.
  CameraList
Manages the list of cameras.
  CommunicationWithParent
Provides ipc and rpc interfaces to the parent when used as a child process.
  ComplexExpression
Interface to a complex expression.
  EmSubprocessIpc
IPC interface between a parent and a child process (used by both sides)
  EmSubprocessRpc
RPC interface between a parent and a child process (used by both sides).
  EmSubprocessRpcMeta
EmSubprocessRpc wrapper which reads the name of a <method> element in the <call> and dispatches it to a slot of a QObject registered for that method.
  Expression
Interface to an expression.
  Parameter
No documentation available.
  Script
Set of instructions that get executed by the interpreter.
  ScriptList
Manages the list of scripts.
  Selectable
Interface to a selectable objects.
  SelectableList
No documentation available.
  Shortcut
Shortcuts are a mechanism to refer to a another Selectable and store that into the project for later use.
  ShortcutGroup
A Shortcutgroup is a collection of Shortcuts.
  ShortcutToInstance
No documentation available.
  ShortcutTree
A Shortcutgroup is a tree of ShortcutTrees.
  Updatable
No documentation available.
  Validity
Reports status of the validity of objects.