Package empro :: Module empro :: Module core :: Class Camera
[frames] | no frames]

Class Camera

A virtual camera object. A camera object can be moved around and tilted to change the view of the current geometry view. The cameras can also be stored in the CameraList for later retrieval.

Class Hierarchy for Camera
Class Hierarchy for Camera

Properties
floatNone fieldHeight
The height of the field of view.
floatNone fieldWidth
The width of the field of view.
Vector3dNone position
The absolute world position of the camera.
Vector3dNone target
The location to where the camera is pointed.
Vector3dNone upVector
The direction that represents the up direction for the camera.