| Home | Trees | Indices | Help |
|
|---|
|
|
core.Updatable --+
|
GridParameters
Interface to optional parameters for the grid.
|
| Class Hierarchy for GridParameters |
| Instance Methods | |
|
Inherited from |
| Properties | |
| CellSizesSpecificationNone |
cellSizes Specification of the cell sizes used for the grid region. |
| stringNone |
gridRegionDirections Specifies in which directions a grid region should be used. |
| Property Details |
gridRegionDirectionsSpecifies in which directions a grid region should be used. Possible values are {'X','Y','Z'}. For example, 'X | Z' specifies that a grid region should be used in the X and Z-direction.
|
| Home | Trees | Indices | Help |
|
|---|
| Generated by Epydoc 3.0.1 on Wed Jun 26 10:16:45 2019 | http://epydoc.sourceforge.net |